Topic: 112

Monitoring Parameters (P0.xxx)

The table below contains basic overview information about the SureServo2 system's Monitoring parameters (P0.xxx). For detailed parameter information, you can access the SureServo2 user manual's parameter section by clicking the link below:

Click here to open Monitoring Parameter details

You can search within the manual using CTRL+F to find the specific parameter. Click BACK to return to the overview page.

Param. No. Function Range Run Read/Write Address Default
P0.000 Firmware version n/a Read 0000H
0001H
Factory Setting
P0.001 Current drive alarm code 0X0000: alarm clear (same as DI.ARST).
0x0001–0xFFFF: displays the alarm code (not writable)
Read/Write■ 0002H
0003H
-
P0.002 LED Display Definition -300 to +127 Read/Write 0004H
0005H
0
P0.003 Analog output monitoring 0–77 Read/Write 0006H
0007H
0x0000
P0.004 Reserved – – – –
P0.005 Reserved – – – –
P0.006 Reserved – – – –
P0.007 Reserved – – – –
P0.008 Total servo drive operation time 0–FFFFFFFF hours Read 0010H
0011H
0
P0.009 Status monitoring register 1 – Read■ 0012H
0013H
0
P0.010 Status monitoring register 2 – Read■ 0014H
0015H
0
P0.011 Status monitoring register 3 – Read■ 0016H
0017H
0
P0.012 Status monitoring register 4 – Read■ 0018H
0019H
0
P0.013 Status monitoring register 5 – Read■ 0020H
0021H
0
P0.014 Reserved – – – –
P0.015 Reserved – – – –
P0.016 Reserved – – – –
P0.017 Select content displayed by status monitoring register 1 0–127 Read/Write 0022H
0023H
0
P0.018 Select content displayed by status monitoring register 2 0–127 Read/Write 0024H
0025H
0
P0.019 Select content displayed by status monitoring register 3 0–127 Read/Write 0026H
0027H
0
P0.020 Select content displayed by status monitoring register 4 0–127 Read/Write 0028H
0029H
0
P0.021 Select content displayed by status monitoring register 5 0–127 Read/Write 002AH
002BH
0
P0.022 Reserved – – – –
P0.023 Reserved – – – –
P0.024 Reserved – – – –
P0.025 Mapping parameter #1 Determined by the corresponding parameter P0.035 Read/Write■ 0032H
0033H
–
P0.026 Mapping parameter #2 Determined by the corresponding parameter P0.036 Read/Write■ 0034H
0035H
–
P0.027 Mapping parameter #3 Determined by the corresponding parameter P0.037 Read/Write■ 0036H
0037H
–
P0.028 Mapping parameter #4 Determined by the corresponding parameter P0.038 Read/Write■ 0038H
0039H
–
P0.029 Mapping parameter #5 Determined by the corresponding parameter P0.039 Read/Write■ 003AH
003BH
–
P0.030 Mapping parameter #6 Determined by the corresponding parameter P0.040 Read/Write■ 003CH
003DH
–
P0.031 Mapping parameter #7 Determined by the corresponding parameter P0.041 Read/Write■ 003EH
003FH
–
P0.032 Mapping parameter #8 Determined by the corresponding parameter P0.042 Read/Write■ 0040H
0041H
–
P0.033 Reserved – – – –
P0.034 Reserved – – – –
P0.035 Target setting for mapping parameter P0.025 Determined by the communication address of the parameter group Read/Write 0046H
0047H
–
P0.036 Target setting for mapping parameter P0.026 Determined by the communication address of the parameter group Read/Write 0048H
0049H
–
P0.037 Target setting for mapping parameter P0.027 Determined by the communication address of the parameter group Read/Write 004AH
004BH
–
P0.038 Target setting for mapping parameter P0.028 Determined by the communication address of the parameter group Read/Write 004CH
004DH
–
P0.039 Target setting for mapping parameter P0.029 Determined by the communication address of the parameter group Read/Write 004EH
004FH
–
P0.040 Target setting for mapping parameter P0.030 Determined by the communication address of the parameter group Read/Write 0050H
0051H
–
P0.041 Target setting for mapping parameter P0.031 Determined by the communication address of the parameter group Read/Write 0052H
0053H
–
P0.042 Target setting for mapping parameter P0.032 Determined by the communication address of the parameter group Read/Write 0054H
005H
–
P0.043 Reserved – – – –
P0.044 Reserved – – – –
P0.045 Reserved – – – –
P0.046 Commonly used DO function status 0x00–0xFF Read■ 005CH
005DH
0x0000
P0.049 Update encoder absolute position registers 0x00–0x02 Read/Write 0062H
0063H
0x0000
P0.050 Absolute coordinate system status 0x00–0x1F Read■ 0064H
0065H
0x0000
P0.051 Encoder absolute position - Number of turns -32786 to +32767 rev Read■ 0066H
0067H
0
P0.052 Encoder absolute position - Pulse number or PUU within single turn 0–16777216-1 (pulse)
-2147483648 to +2147483647 (PUU)
Read■ 0068H
0069H
0
P0.053 General range compare DO output - Filter time 0x0000–0x000F ms Read/Write 006AH
006BH
0x0000
P0.054 General range compare DO output - lower limit -2147483648 to +2147483647 Read/Write 006CH
006DH
0
P0.055 General range compare DO output - upper limit -2147483648 to +2147483647 Read/Write 006EH
006FH
0
P0.056 General range compare DO - second lower limit -2147483648 to +2147483647 Read/Write 0071H
0072H
–
P0.057 General range compare DO - second upper limit -2147483648 to +2147483647 Read/Write 0073H
0074H
–
P0.058 General range compare DO - third lower limit -2147483648 to +2147483647 Read/Write 0075H
0076H
–
P0.059 General range compare DO - third upper limit -2147483648 to +2147483647 Read/Write 0077H
0078H
–
P0.060 General range compare DO - fourth lower limit -2147483648 to +2147483647 Read/Write 0079H
007AH
–
P0.061 General range compare DO - fourth upper limit -2147483648 to +2147483647 Read/Write 007BH
007CH
–
P0.062 Reserved – – – –
P0.063 Duration of DC Bus voltage exceeding 400V 0x00000000 to 0x7FFFFFFF ms Read/Write 007EH
007FH
0
P0.064 Reserved – – – –
P0.065 Reserved – – – –
P0.066 Reserved – – – –
P0.067 Reserved – – – –
P0.068 Reserved – – – –